Measured parameters
- EnergyThe meter provides bi-directional, 4-quadrant, Class 1 / Class 0.5S accurate energy metering.The meter provides bi-directional, 4-quadrant, Class 0.5S accurate energy metering.The meter provides bi-directional, 4-quadrant, Class 1 / Class 0.5S / Class 0.2 accurate energy metering.The meter provides bi-directional, 4-quadrant, Class 1 / Class 0.5S accurate energy metering.
- Non Reset energyNon Reset energy parameters are Wh, VAh and VARh for both Del and Rec. Non Reset energy parameters are available on display in Diag page under Maintenance and through communication..
- DemandThe meter provides last, present, predicted, and maximum (peak) demand values, and a timestamp when the maximum (peak) demand occurred.
- InstantaneousThe meter provides highly accurate 1-second measurements, average values, including true RMS, per phase and total for:
- Power qualityThe meter provides complete harmonic distortion measurement, recording, and real-time reporting, up to the 15th harmonic for PM2220PM2220R and up to 31st harmonic for PM2230PM2230R for all voltage and current inputs.
- Data recording (PM2230PM2230R)The meter stores each new minimum and new maximum value with date and timestamp for all instantaneous values (average, total, and each phase).
- Input/output (PM2230PM2230R)The meter supports optional input and output capabilities.
- Other measurementsAdditional measurements recorded by the meter include several timers.
Parent topic: Introduction