Enabling/Disabling communication protocols

Disabling unnecessary and unused communication protocols such as BACnet/IP reduces the attack surface. Changing the port number default values reduces the predictability of use.

Configuring BACnet/IP settings using the display

See Configuring BACnet/IP settings using the display for instructions on how to enable/disable BACnet/IP configuration on your device using the display.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?