Configuring BACnet/IP settings using the display

Use the meter’s display to configure BACnet/IP settings if required.
  1. Navigate to Maint > Setup .
  2. Enter the setup password (default is “0”),then press OK.
  3. Navigate to Comm > BACnet .
  4. Move the cursor to point to the parameter you want to modify, then press Edit.
  5. Modify the parameter as required, then press OK.
  6. Move the cursor to point to the next parameter you want to modify, press Edit, make your changes, then press OK.
  7. Press the up arrow to exit.

    Basic BACnet/IP settings available using the display

    Parameter Values Description

    BACnet Status

    Enabled, Disabled

    Enable or disable BACnet/IP communications with the meter

    Device ID

    1 – 4194302

    Enter the ID of the meter on your BACnet network. The ID must be unique on the network.

    UDP Port

    1024 – 65535

    Enter the port the meter uses for BACnet/IP communications. The default is the standard BACnet/IP port (47808).

    Foreign device settings available using the display

    Parameter Values Description

    BBMD Status

    Enabled, Disabled

    Enable or disabled registration of the meter as a foreign device.

    BBMD IP

    Contact your local network administrator for parameter values.

    Enter the IP address of the BACnet/IP Broadcast Management Device (BBMD), if you use a BBMD on your network.

    BBMD Port

    1024 – 65535

    Enter the port number that is used for communications with the BBMD. The default is the standard BACnet/IP port (47808)

    BBMD TTL (sec)

    0 – 65535

    The length of time (in seconds) the BBMD keeps an entry for this device in its foreign device table.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?