Panel-mount meter mounting and wiring recommendations

There are supplemental mounting and wiring recommendations that apply to panel-mount meters.
  • The meter is intended to be mounted inside a ΒΌ-DIN panel cutout.

  • Inspect the gasket (installed around the perimeter of the display) and make sure it is secured properly and not damaged.

  • The meter retainer clips, located on either side of the meter base and used to secure the meter in the panel, do not usually require any tools to install.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?