Direct connect voltage limits

You can connect the meter’s voltage inputs directly to the phase voltage lines of the power system if the power system’s line-to-line or line-to-neutral voltages do not exceed the meter’s direct connect maximum voltage limits.

The meter's voltage measurement inputs are rated by the manufacturer for up to 400 V L-N / 690 V L-L. However, the maximum voltage allowed for direct connection may be lower, depending on the local electrical codes and regulations. In US and Canada the maximum voltage on the meter voltage measurement inputs may not exceed 347 V L-N / 600 V L-L.

If your system voltage is greater than the specified direct connect maximum voltage, you must use VTs (voltage transformers) to step down the voltages.

Power system description

Meter setting

Symbol

Direct connect maximum (UL)

Direct connect maximum (IEC)

# of VTs (if required)

Single-phase 2-wire line-to-neutral

1PH2W LN

347 V L-N

400 V L-N

1 VT

Single-phase 2-wire line-to-line

1PH2W LL

600 V L-L

690 V L-L

1 VT

Single-phase 3-wire line-to-line with neutral

1PH3W LL with N

347 V L-N / 600 V L-L

400 V L-N / 690 V L-L

2 VT

3-phase 3-wire Delta ungrounded

3PH3W Dlt Ungnd

600 V L-L

600 V L-L

2 VT

3-phase 3-wire Delta corner grounded

3PH3W Dlt Crnr Gnd

600 V L-L

600 V L-L

2 VT

3-phase 3-wire Wye ungrounded

3PH3W Wye Ungnd

347 V L-N / 600 V L-L

400 V L-N / 690 V L-L

2 VT

3-phase 3-wire Wye grounded

3PH3W Wye Gnd

347 V L-N / 600 V L-L

400 V L-N / 690 V L-L

2 VT

3-phase 3-wire Wye resistance-grounded

3PH3W Wye Res Gnd

347 V L-N / 600 V L-L

400 V L-N / 690 V L-L

2 VT

3-phase 4-wire open Delta center-tapped

3PH4W Opn Dlt Ctr Tp

347 V L-N / 600 V L-L

400 V L-N / 690 V L-L

3 VT

3-phase 4-wire Delta center-tapped

3PH4W Dlt Ctr Tp

347 V L-N / 600 V L-L

400 V L-N / 690 V L-L

3 VT

3-phase 4-wire ungrounded Wye

3PH4W Wye Ungnd

347 V L-N / 600 V L-L

400 V L-N / 690 V L-L

3 VT or 2 VT

3-phase 4-wire grounded Wye

3PH4W Wye Gnd

347 V L-N / 600 V L-L

400 V L-N / 690 V L-L

3 VT or 2 VT

3-phase 4-wire resistance-grounded Wye

3PH4W Wye Res Gnd

347 V L-N / 600 V L-L

400 V L-N / 690 V L-L

3 VT or 2 VT

NOTE:
  • Use a 500 mA fuse or a circuit breaker for the meter voltage input terminals.

  • Use a shorting block between the current transformer (CT) and the meter current input terminals.

  • Use primary fuses and disconnect switch to protect the potential transformer (PT).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?