Energy pulsing

You can configure the meter’s alarm /energy LED or the digital output(s) for energy pulsing.

  • The meter is equipped with an alarm / energy pulsing LED. When configured for energy pulsing, the LED emits pulses that are then used to determine the accuracy of the meter’s energy measurements.

  • The meter sends the pulses from the configured digital output(s) port, which are then used to determine the accuracy of the meter’s energy measurements by pulse counter.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?