Diagnostics information

The diagnostics screen provides meter information, status and event data for troubleshooting.

Navigate to Maint > Diag > Meter to view details of the meter status.

Navigate to Maint > Diag > Cl Pwr to view the control power information.

  • Non-MID/MIR meter models : The Cl Pwr screen displays how many times the meter lost control power, and the date and time of its last occurrence.

  • MID/MIR meter models : The Cl Pwr screen displays how many times the meter lost control power (auxiliary power), and the last power up and power down events with the timestamp.

Navigate to Maint > Diag > PhAng to view the graphical representation of the power system the meter is monitoring.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?