MTN6194-6010S_SW_24_06_14

KNX Data Secure

The KNX standard has been extended by KNX Data Secure to protect KNX installations from unauthorized access. KNX Data Secure reliably prevents the monitoring of communication and manipulation of the installation. KNX Data Secure describes the encryption at telegram level so that communication via objects is encrypted and therefore secure.

Encrypted telegrams are longer than the previously used unencrypted telegrams. For secure programming via the KNX bus, it is therefore necessary for the interface (e.g. USB) and any line couplers to support these „KNX long frames“.

Special conditions must be observed when using secure devices in the ETS. Please refer to the relevant web pages on the KNX website https://www.knx.org

Protecting your data is a top priority. Use the options in the ETS and KNX Data Secure to protect your data, configuration and installations from unauthorized access.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?