MTN6194-6010S_SW_24_06_14

RGB Color Codes

On each color scale (Red, Green, Blue) it is possible to select 256 levels or shades of the appropriate color (from 0 to 255). By mixing them together you can generate over 16 million different color combinations.

RGB value

If you know the specific color code, you can simply write it directly in the RGB value box. The box is immediately colored according to the entered value.

The second option is to click on the color window icon at the bottom right and use the cursor to select a color on the color scale.

RGB colors

The following table shows the values for the basic RGB colors.

Red

Green

Blue

Color

255

0

255

Pink

255

0

0

Red

255

127

0

Orange

255

255

0

Yellow

127

255

0

Green-yellow

0

255

0

Green

0

255

255

Blue-green

0

0

255

Blue

255

255

255

White

NOTE: The colors may be displayed differently, depending on the color control device and the lamps being used.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.