DOCA0238ZH-01

软件要求

TeSys island DTM 库要求电脑上安装以下软件:

  • Microsoft .NET Framework v3.5 SP1

  • EcoStruxure Control Expert v15.0 SP1 或 EcoStruxure Machine Expert v1.2.7 或更高版本或 SoMove v2.9

  • Modbus DTM Library v2.6.12 或更高版本

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?