DOCA0224EN-06

Version 003.002.000

New Features

  • Configurable Fallback Mode

    For starters and IO module outputs, the fallback position can be configured for each avatar except Power Interface avatar.

  • Korean language support

    Korean language is supported in SoMove and Operation and Maintenance Tool (OMT).

  • Avatar trip status for IO PORT ASSIGNMENT

    IO PORT ASSIGNMENT table lists avatar trip status and individual trip status, which can be assigned to digital outputs.

  • Configurable communication loss timeout for Fieldbus Protocol

    Communication loss timeout can be configured for the Fieldbus Protocol.

Bugs Fixed

Positive Temperature Coefficient (PTC) Binary as Process Variable (PV) input.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?