Version 003.000.002
-
Perform an upgrade from 001.100.013/002.100.016 to 002.200.008/002.300.006.
-
Perform an upgrade from 002.200.008/002.300.006 to 003.000.002.
New Features
-
avatar in IO Optimization
feature allows users to share their I/O devices between different avatars and optimize them to reduce the number of I/O devices required per TeSys island.
User may also utilize feature which will permanently remove free AIOM/DIOM devices from the TeSys island configuration.
-
FLA can be configured through Modbus TCP registers.
Bugs Fixed
When the emergency push button is pressed, all of the modules will not have power in TeSys island.
Known Issues
-
In IO PORT ASSSIGNMENT, if analog input type is different from analog output type and when analog input is connected to analog output, avatar device event occurs.
Workaround: Use same type of analog input and analog output.
-
Communication cannot be established between Ecostruxure Control Expert and TeSys island, if there are 15 or more avatars in an TeSys island configuration.