Version 003.001.001
New Features
Korean language support.
KC (Korean Certification) will be applicable to the below commercial references:
|
In scope |
|
|---|---|
|
TPRBCEIP |
Ethernet/IP bus coupler |
|
TPRBCPFN |
PROFINET bus coupler |
|
TPRDG4X2 |
Digital I/O module |
|
TPRST009 |
9 A standard starter |
|
TPRST025 |
25 A standard starter |
|
TPRST038 |
38 A standard starter |
|
TPRST065 |
65 A standard starter |
|
TPRST080 |
80 A standard starter |
|
TPRVM001 |
Voltage interface module |
|
TPRAN2X1 |
Analog I/O module |
|
Out of scope |
|
|---|---|
|
TPRBCPFB |
PROFIBUS bus coupler |
|
TPRPM009 |
9 A Power inteface module |
|
TPRPM038 |
38 A Power inteface module |
|
TPRPM080 |
80 A Power inteface module |
|
TPRSM001 |
SIL interface module |
|
TPRSS009 |
9 A SIL starter |
|
TPRSS025 |
25 A SIL starter |
|
TPRSS038 |
38 A SIL starter |
|
TPRSS065 |
65 A SIL starter |
|
TPRSS080 |
80 A SIL starter |