Safety Information
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
WARNING |
|---|
|
UNINTENDED EQUIPMENT OPERATION
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
| NOTICE |
|---|
|
RISK OF FIRMWARE CORRUPTION
Updating the firmware on TeSys T controller through the
programmer provides an automatic restore function for the product
configurations. Before changing the firmware version, it is recommended
to save a backup of the product configuration through the TeSys T
Device Type Manager (DTM) using SoMoveTM Software.
Once programming has begun, adhere to the following until the programming process is complete:
Failure to follow these instructions can result in equipment damage.
|
|
|
WARNING: This product can expose you to chemicals including lead and lead compounds, which are known to the State of California to cause cancer and birth defects or other reproductive harm. For more information go to www.P65Warnings.ca.gov. |
DANGER
WARNING