Introducing the TeSys T Motor Management System
Presentation of the TeSys T Motor Management System
Aim of the Product
The TeSys T motor management system offers protection, control, and monitoring capabilities for single-phase and three-phase AC induction motors.
The system is flexible, modular, and can be configured to meet the requirements of applications in industry. The system is designed to meet the needs for integrated protection systems with open communications and a global architecture.
Highly accurate sensors and solid-state full motor protection provide better utilization of the motor. Complete monitoring functions enable analysis of motor operating conditions and faster responses to minimize system downtime.
The system offers diagnostic and statistics functions and configurable indications and detected conditions, allowing better prediction of component maintenance, and provides data to continuously improve the entire system.
For more details on the product, refer to the TeSys T LTMR Motor Management Controller User Guide.
Firmware Update Policy
Firmware update is recommended to benefit from the latest features and potential bug fixes. Update the firmware to the latest version when the latest features and bug fixes are required for your application. Use the firmware release notes to confirm if an update to the latest version of the firmware is relevant for your application. The latest firmware and release notes can be found together by searching for "TeSys T Firmware" at www.se.com.
Firmware Update with TeSys Programmer
Use the latest version of TeSys Programmer software to update the TeSys T range of devices with the latest firmware version available. The latest version of TeSys Programmer software is available at www.se.com. For more information on the use of TeSys Programmer software, refer to TeSys Programmer Help document that is provided with the software.