DOCA0260EN-00

Firmware Update

Update the TeSys Tera system to the latest firmware version to obtain the latest features and keep up-to-date with security patches. All firmware designed for the TeSys Tera system is signed using the Schneider Electric Public Key Infrastructure (PKI) to help provide integrity and authenticity of the firmware running on the TeSys Tera system.

For more information about the firmware update through TeSys Tera DTM, refer to TeSys Tera Motor Management System DTM Library Online Help Guide – DOCA0275EN.

For more information about the firmware update through the standard web server (applicable for Ethernet interface modules), refer to TeSys Tera Motor Management System EtherNet/IP Communication Guide - DOCA0258EN.

To know more on the security updates, register with the Security Notifications on Schneider Electric Cybersecurity Support Portal.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.