DOCA0260EN-00

Physical Security

Installation

To help protect the systems physical security, the following installation is advised:

  • Install the TeSys Tera system in an enclosure that is secured in a manner appropriate to the risk level of your installation (for example, an enclosure with a padlock or a key).

  • If the TeSys Tera system is mounted on a switchboard, install the switchboard in a secured room (for example, with a locked door or camera).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.