辅助触点接线

有关辅助触点的安装信息,请参阅 Schneider Electric 网站上的说明书:

  • TransferPacT Active Automatic / Automatic 32-100 A:JYT3049801

  • TransferPacT Active Automatic / Automatic 80-160 A:JYT3049901

  • TransferPacT Active Automatic / Automatic / Remote 100–250 A:GEX2525501

  • TransferPacT Active Automatic / Automatic / Remote 320–630 A:GEX2525601

  • TransferPacT Active Automatic / Automatic / Remote 800 A:BQT1751501

  • TransferPacT Active Automatic 800–1600 A:BQT7680301

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

这有帮助吗?