Coding Principle

The commercial reference of Automatic Transfer Switching Equipment (ATSE) and Remote Transfer Switching Equipment (RTSE) are coded with significant features to explain the type of frame ratings, transition type, controller type, rated voltage, rated current, and number of poles.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?