Compression Lug

DANGER
hazard of electric shock, explosion or arc flash
  • It is mandatory to install interphase barrier.
  • It is mandatory to use the screws provided in the switch packaging box.
  • For aluminum lugs with interphase barriers, it is mandatory to install front insulating screen or custom made fiber insulating plate.
  • For copper lugs two cable connection, it is mandatory to install rear insulating screen or custom made fiber insulating plate.
Failure to follow these instructions will result in death or serious injury.
WARNING
Hazard of fire
  • Use only specified wiring cross-section with the equipment and comply with the specified wiring requirements.
  • Tighten the connections with the specified torque value.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The compression lugs are screwed on the switch using the screws delivered with the switch.

The table below provides the list of the compression lugs:

Switch

Number of poles

Material

Compression lug

Frame 250 : 100–250 A

3P

Cu

LV429252

LV429253

LV429254

Al

LV429504

LV429506

4P

Cu

LV429256

LV429257

LV429258

Al

LV429505

LV429507

Frame 630: 320–630 A

3P

Cu

TPSCON57

TPSCON59

Al

TPSCON61

TPSCON63

4P

Cu

TPSCON58

TPSCON60

Al

TPSCON62

TPSCON64

Frame 800: 800 A

3P

Cu

TPSCON57

TPSCON59

4P

Cu

TPSCON58

TPSCON60

For information on installation, consult the instruction sheets on Schneider Electric website:

  • TransferPacT Active Automatic / Automatic / Remote 100–250 A: GEX2525501

  • TransferPacT Active Automatic / Automatic / Remote 320–630 A: GEX2525601

  • TransferPacT Active Automatic / Automatic / Remote 800 A: BQT1751501

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?