Fire Protections 24 V DC Pulse Input

The fire protection is an accessory module installed on TransferPacT Automatic and TransferPacT Active Automatic controller with following functions:

  • Exit the auto transfer mode and transfer the switch to OFF according to input signal.

  • Fire protection with input of DC 24 V pulse signal.

  • Green LED on the front face of the accessory indicates the power status and proper connection of the accessory.

  • The main MCU on ATSE communication through CAN bus.

  • Only one module is allowed to be installed on one product.

Application

When there is fire emergency, the fire protection signal can transfer ATSE to off position.

Terminals

  • Fire protection with 24 V DC Pulse:

    • Start: P1+.P1-

    • Exit: P2+,P2-

Performance

Electrical characteristics

Ratings

Ui

30 V DC

Maximum input voltage (fire enable)

28.8 V DC

Minimum input voltage (fire enable)

19.2 V DC

Maximum input voltage (fire disable)

28.8 V DC

Minimum input voltage (fire disable)

19.2 V DC

Maximum input current

10 mA

Over voltage category

II

Pollution degree

3

Altitude

2000 m

Cable Capacity for Terminals

The cable capacity for the terminals are 0.05 – 2.6 mm2 (AWG 30 ~ 13).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?