Acronyms and Terminology

Short terms

Expansion

Description

TSE

Transfer Switching Equipment

Self-acting transfer switching equipment, including all necessary sensing inputs, monitoring, and control logic for transferring operations.

ATSE

Automatic Transfer Switching Equipment

RTSE

Remote Transfer Switching Equipment

Remote operated transfer switching equipment

MTSE

Manual Transfer Switching Equipment

Manually operated transfer switching equipment

SI

Source I

SI supply

SII

Source II

SII supply

N

Normal

Normal supply

A

Alternate

Alternate supply

E

Emergency

 

O

Off position

Two powers are disconnected

Specific TSE

Specific transfer switching equipment

2/3 position dedicated designed as IEC 60947-6-1 product requirement

Derived TSE

Derived transfer switching equipment

Fulfilling requirements of other IEC 60947 product standards

Open transition

Normal transfer

The basic transfer function

In phase transition

Sync transition

Open transition but detect phase angle when re-transfer

Delayed transition

Delay transition

A programmable time delay for neutral position

Close transition

Close transition

A load transfer by momentarily paralleling both sources

Neutral overlapping

Transfer with neutral overlapping

Making before breaking and N will never be lost

Under voltage sensor

 

Detect the Undervoltage of power source

Over voltage sensor

 

Detect the Overvoltage of power source

Frequency sensor

 

Detect the frequency of power source

Voltage imbalance sensor

 

Detect the balance of power source

Phase rotation sensor

 

Detect the phase angle of power source

Loss of single-phase sensor

 

Detect the phase of power source

T2

Transfer Delay

Transfer delay

T4

Center-off Delay

Center-off delay

T6

Re-Transfer Delay

Re-Transfer Delay

T7

Genset Start Delay

Genset start delay

T8

Loadshed Delay

Loadshed delay

T9

Genset Cool Delay

Genset cool delay

T10

Genset Fail Delay

Genset fail delay

T13

On Load Test Delay

On load test delay

T14

Off Load Test Delay

Off load test delay

Power supply models

 

An additional power supply connection for controller

Auto-return

 

A working mode for ATSE controller

Non-return

 

A working mode for ATSE controller

Manual-return

 

A working mode for ATSE controller

Load shed

 

A signal from ATSE controller to shed the load

Transfer inhibit

 

Override transfer orders

Genset start

 

A Genset start signal from controller

Fire protection

 

Shed the ATSE when fire signal is received

Voluntary remote control

 

Transfer remotely

External 24 Vdc

 

External power for controller/communication

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?