Dielectric Test

Dielectric Test Switch

NOTICE
HAZARD OF EQUIPMENT DAMAGE
  • Before dielectric test, put the dielectric switch to test position to turn off the controller.
  • After the dielectric test, put the dielectric switch back to run position to power on the controller.
Failure to follow these instructions can result in equipment damage.

The dielectric switch on the controller is used to disconnect the controller before performing the dielectric test and install accessory. Both functions are needed to disconnect dielectric switch. The arrow position of the switch indicates whether the controller is disconnected (Test) or connected (Run) to perform the dielectric test.

Perform the following procedure for dielectric test:

  1. Insert the screwdriver and rotate anti-clockwise to bring it to Test position.

  2. Perform the dielectric test once the dielectric switch is ejected.

  3. Insert the screwdriver and rotate the dielectric switch clockwise to bring it to Run position after the dielectric test.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?