Modbus Functions

General Description

The Modbus protocol offers a number of functions that are used to read or write data over the Modbus network. The Modbus protocol also offers diagnostic and network-management functions.

Only the Modbus functions handled by the ATSE are described here.

Read Functions

The following read functions are available:

Function Code

Subfunction Code

Name

Description

3 (0x03)

Read holding registers

Read n output or internal registers

43 (0x2B)

14 (0x0E)

Read device identification

Read the identification data of the server

43 (0x2B)

15 (0x0F)

Get date and time

Read the date and time of the server

Read Register Example

The following table shows how to read the SI voltage in register 2000. The address of register 2000 is 2000-1=1999 = 0x07CF. The Modbus address of the Modbus server is 47 = 0x2F.

Client Request

Server Reply

Field Name

Example

Field Name

Example

Modbus server address

0x2F

Modbus server address

0x2F

Function code

0x03

Function code

0x03

Address of the register to read (MSB)

0x07

Data length in bytes

0x02

Address of the register to read (LSB)

0xCF

Register value (MSB)

0x02

Number of registers (MSB)

0x00

Register value (LSB)

0x2B

Number of registers (LSB)

0x01

CRC (MSB)

0xXX

CRC (MSB)

0xXX

CRC (LSB)

0xXX

CRC (LSB)

0xXX

Get Date and Time Example

The following table shows how to get the date and time of a Modbus server. The Modbus address of the Modbus server is 47 = 0x2F.

client Request

Server Reply

Field Name

Example

Field Name

Example

Modbus server address

0x2F

Modbus server address

0x2F

Function code

0x2B

Function code

0x2B

Subfunction code

0x0F

Subfunction code

0x0F

Reserved

0x00

Reserved

0x00

Date and time

Refer to the DATETIME data type

Set Date and Time Example

The following table shows how to set date and time of a Modbus server. The Modbus address of the Modbus server is 47 = 0x2F, the new date is October 2, 2014, and the new time is 2:32:03:500 p.m.

NOTE: Use the broadcast mode (with Modbus server address = 0) to set the date and time of all Modbus servers.

client Request

Server Reply

Field Name

Example

Field Name

Example

Modbus server address

0x2F

Modbus server address

0x2F

Function code

0x2B

Function code

0x2B

Subfunction code

0x10

Subfunction code

0x10

Reserved1

0x00

Reserved1

0x00

Not used

0x00

Not used

0x00

Year = 2014

0x0E

Year = 2014

0x0E

Month = October

0x0A

Month = October

0x0A

Day Of Month = 2

0x02

Day Of Month = 2

0x02

Hour = 14

0x0E

Hour = 14

0x0E

Minutes = 32

0x20

Minutes = 32

0x20

3 sec. 500 ms

0x0DAC

3 sec. 502 ms

0x0DAE

The normal response is an echo of the request, returned after the date-time has been updated in the remote device. If the date-time structure content is not consistent with a true date-time (that is, an invalid date-time), the value returned in the Date-Time field is set to 0 by the device.

In case of 24 VDC power loss, the date and time of the Modbus servers without battery is not refreshed anymore. It is therefore mandatory to set date and time for all Modbus servers after recovering the 24 VDC power supply.

Furthermore, due to the clock drift of each Modbus server, it is mandatory to set date and time for all Modbus servers periodically. Recommended period is at least every 15 minutes.

Scattered Holding Register Read Function

The scattered holding register read function is available:

Function

Subfunction Code

Name

Description

100 (0x64)

4 (0x04)

Read scattered holding register

Read n non-contiguous registers

The scattered holding register read function enables the user to:

  • avoid reading a large block of contiguous registers when only few registers are needed

  • avoid multiple use of functions 3 and 4 in order to read non-contiguous registers

Read Scattered Holding Register Example

The following table shows how to read the addresses of the register 1022 (address 0x03FD) and register 1100 (address 0x044B) of a Modbus server. The Modbus address of the Modbus server is 47 = 0x2F.

Client Request

Server Reply

Field Name

Example

Field Name

Example

Modbus server address

0x2F

Modbus server address

0x2F

Function code

0x64

Function code

0x64

Data length in bytes

0x06

Data length in bytes

0x06

Subfunction code

0x04

Subfunction code

0x04

Transmission number(1)

0xXX

Transmission number(1)

0xXX

Address of first register to read (MSB)

0x03

Value of the first register read (MSB)

0x12

Address of first register to read (LSB)

0xFD

Value of the first register read (LSB)

0x0A

Address of second register to read (MSB)

0x04

Value of the second register read (MSB)

0x74

Address of second register to read (LSB)

0x4B

Value of the second register read (LSB)

0x0C

CRC (MSB)

0xXX

CRC (MSB)

0xXX

CRC (LSB)

0xXX

CRC (LSB)

0xXX

(1) The client gives the transmission number in the request. The server returns the same number in the reply.

Write Functions

The following write functions are available:

Function Code

Subfunction Code

Name

Description

6 (0x06)

Preset single register

Write 1 register

16 (0x10)

Preset multiple registers

Write n registers

43 (0x2B)

16 (0x10)

Set date and time

Write the date and time of the server

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?