Open Transition

Open transition is a process to break before the transfer operation. It is done intentionally to break the load current from one source prior to making it to the other source, such that the load is not supplied for a period of time.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?