TransferPacT Transfer Switching Equipment Overview

TransferPacT ATSE is provided with an advanced microprocessor controller with two options:

  • Active automatic HMI (LCD display and keypad)

  • Automatic HMI (Rotary and DIP switch)

It is a robust and reliable controller which offers all of the voltage, frequency, control, timing and diagnostic functions required for wide range of power applications.

The Automatic HMI is easy to install and use, while Active Automatic HMI contains every function needed with eight control modes.

There are two key features of TransferPacT ATSE controller:

  • Automatic HMI can be hot swapped to Active Automatic HMI, an easy way to upgrade your controller. HMI can also be easily replaced for maintenance or renewal.

  • 10 types of function modules can be installed on TransferPacT ATSE controller at any time, which provides maximum scalability, reduced total cost of ownership, and add functions with growing demands..

TransferPacT RTSE has intelligent control with CPU integrated in switch, it is provided with:

  • Input and output terminals

Besides the terminals for I/O signals, it also provides power state, product state and alarm indication through LED indicator on product front face.

TransferPacT RTSE is designed to manage the transfer according to the incoming command of the third party. It can work with third party system, like generator-set controllers, PLCs etc.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?