PowerTag

The PowerTag can be mounted on the 4–pole TransferPacT Active Automatic / Automatic / Remote 100-250 A transfer switch equipment load side.

To install the PowerTag M250 on the Transfer switching equipment, consult the instruction sheet QGH46820.

Switch

Number of poles

PowerTag

Frame 250: 100–250 A

4P

LV434021

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?