Quick Menu Tour

The location of some frequently used menus are listed in the following table. You can also find the default setting of these item.

Menu

Sub-menu 1

Sub-menu 2

Range

Default

System Param

Rated Voltage

-

please refer to System Parameters Sub-Page

Ue-220V: 230V, or

Ue-400V: 400V, or

Ue-208V: 230V, or

Rated Frequency

-

50 Hz; 60 Hz

50 Hz

Neutral position

-

NABC; ABCN

NABC

Application

Source Config

-

S1 Utility(N) - SII Genset(A);
S1 Utility(A) - SII Utility(N);
S1 Utility(N) - SII Utility(A);
S1 Genset(A) - SII Utility(N)

S1 Utility(N) - SII Genset (A)

Transfer Conditions

Phase SEQ Warning

ON; OFF

ON (IEC)
OFF (China)

Volt UNB Warning

ON; OFF

OFF

N Wrong Warning

ON; OFF

ON (IEC)
OFF (China)

U > Ue Transfer

ON; OFF

OFF

Abnormal FRQ Trans

ON; OFF

OFF

Gen Start Fail Warning

ON; OFF

OFF

Neutral Loss Transfer

ON; OFF

OFF

Return Modes

-

Auto Return;
Non Return;
Manual Return (China)

Auto Return

SI setpoints

UV dropout

please refer to Application Sub-Page

85 %

UV pickup

90 %

OV dropout

110 %

OV pickup

105 %

UF dropout

96 %

UF pickup

97 %

OF dropout

102 %

OF pickup

101 %

Unbalance rate

2 %-30 %

5 %

SII setpoints

UV dropout

please refer to Application Sub-Page

85 %

UV pickup

90 %

OV dropout

110 %

OV pickup

105 %

UF dropout

96 %

UF pickup

97 %

OF dropout

102 %

OF pickup

101 %

Unbalance rate

2 %-30 %

5 %

Time Delays

Transfer Delay

-

0-1800 s

3 s (IEC)
0 s (China)

Re-Transfer Delay

-

0-3600 s

60 s (IEC)
0 s (China)

Center-off Delay

-

0-30 s

0 s

Loadshed Delay

-

0-15 s

0 s

Gen Start Delay

-

0-120 s

3 s (IEC)
0 s (China)

Gen Cool Delay

-

0-3600 s

60 s (IEC)
0 s (China)

Gen Fail Delay

-

15-300 s

300 s

Settings

Accessories

DI Test (if supported)

ON Load Test;
Off Load Test

ON Load Test

Modbus (if supported)

Address
Baudrate
Parity
Stop bit

Address = 001
Baudrate = 19200
Parity = Even
Stop bit = 2

Quick View Auto Scroll

-

ON (1-300 s); OFF

OFF

Language

-

-

8 languages

English

Date/Time

-

-

YYYY-MM-DD-HH-MM-SS

2000-01-01 00:00:00

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?