Single Line Diagram LED

LED indication

Status

Description

No energy, ATSE power off

ATSE updating in process or in Test mode

ATSE is running in normal operation, ready to transfer

The ATSE is running in Auto mode

The ATSE will be in Not in Automatic mode, and will not automatically transfer in case of source failure.

No alarm

Alarm is active

SI

No Source I

Source I out of range

Source I present and in the range

SII

No Source II

Source II out of range

Source II present and in the range

Source I is opened (Not connected)

Time delay is running for transferring

Source I is closed (Connected)

Source II is opened (Not connected)

Time delay is running for transferring

Source II is closed (Connected)

LED indication

Status

Description

Both sources are out of range, or the transfer switch equipment is in manual/lock mode

Either source is in range and transfer switch equipment is in RUN mode

No alarm

Alarm is active (transfer failure, transfer switch equipment contact position failure, internal error occurred)

NOTE: The LED indicator on the equipment and the external HMI is for reference. In the event of a contradiction between the LED and the position indicator on the ATSE, the latter prevails.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?