Automatic HMI Description

Label

Description

A

Rated frequency

B

Time delay for center-off position

C

Type of sources:

  • Utility/Utility

  • Utility/Genset

D

Source priority

E

Transition mode for return to normal position

F

Rated voltage

G

Voltage and frequency thresholds setting

H

Transfer time delay in seconds from normal source to alternate source

I

Transfer time delay in minutes from alternate source to normal source

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?