Upside-down Installation Kit

Upside-down installation kit can be used to mount the transfer switching equipment in upside-down position on accessibility or space requirements.

The below table provides the list of upside-down installation kit:

Switch

Vertical connection adapter

Frame 1A: 800–1600 A

TPSOTH73

 

For information on installation, consult the instruction sheet on the Schneider Electric website: BQT7680301.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?