Vertical Connection Adapter

Vertical connection adapters are used to adapt the busbar connection of the TransferPacT Active Automatic 800–1600 A transfer switching equipment.

To adapt the cable lug connection on vertical connection adapters, connect the cable-lug adapter on the vertical connection adapter, and then connect the cable lug on the cable-lug adapter. For more information, refer to the Cable-lug Adapter.

Vertical connection adapters are screwed on the switch using the screws delivered with the adapter.

The table below provides the list of the vertical connection adapter:

Switch

Number of poles

Vertical connection adapters

Frame 1A: 800–1600 A

3P

33642 / LV833642SP

4P

33643 / LV833643SP

For information on installation, consult the instruction sheet on Schneider Electric website: BQT7680301 .

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?