Handle Transfer Mode

  • The handle or manual transfer mode is activated from the TSE directly. It deactivates the controller control function except position status (outputs and LEDs), source status LEDs and alarm LED.

  • No operation for load shedding and generator, keep the status as before.

  • No alarm relay output.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?