Ethernet mode connection— Wiser Basic Hub

  1. (See A) Locate the Ethernet port on the Basic Hub.
  2. Connect an Ethernet cable between the Basic Hub gateway and the router to suit the installation method used for the Basic Hub gateway:
    • (See B) Wall surface installation

    • (See C) Smooth surface installation

    • (See D) Table mount

You must add the Basic Hub gateway to the app before you can add devices to control them. To do this, first download and install the app on your mobile phone/tablet (see Downloading the app) and register a user account. You can then add the basic hub gateway and optionally connect the basic hub gateway to the router by Wi-Fi. See Commissioning the Hub and Basic Hub gateway (Ethernet mode).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?