DUG_Puck Relay_LK-00

About the device

The Wiser wireless relay for build in (hereinafter referred to as Puck/Micro Module Light Switch) combines the advantages of smart switch functionality with ordinary mechanical push-button switches. It transforms a conventional switch into a connected device that can be controlled from the switch or through the Wiser app. It can switch ohmic, inductive or capacitive loads.
IMPORTANT: Do not control any devices that depend on a permanent power supply.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?