DUG_Puck Relay_LK-00

Pairing device with auto scan

Pairing the device with auto scan automatically discovers the device when the corresponding device is powered on.
  1. On the Home page, tap +.
  2. Tap Auto scan > Confirm.
  3. Enable permissions to Access location and Wi-Fi for scanning device and tap Start scanning.
    NOTE: If you have multiple hubs, do Step 4 or proceed to Step 5.
  4. Tap Select hub and select the from the slide-up menu.
  5. Short press the setup/reset button 3 times (< 0,5 s) and wait for a few seconds until the device search is complete.
    The LED blinks orange.
    TIP: If you want to pair multiple devices at once, perform step 5 on each device and wait for a few seconds for them to be detected.
  6. Tap Next (A) and select Micromodule Switch.

  7. Once the device is added successfully, tap Done.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?