DUG_Exxact - Blind Control Switch_WSE-00

Example of an automation

This demonstration shows you how to create an automation to open the shutter at the scheduled time.
  1. Go to Automation > + to create an automation.
  2. Tap Edit name , enter the name of the automation and tap Confirm.
    TIP: You can choose the cover image that represents your automation by tapping .
  3. Tap Add Condition > Schedule.
    • Tap Repeat (A), select the days you want to set the schedule and tap Save.

    • Set the time (B) at which the automation must start and tap Next.

  4. Tap Add task > Run the device > Blind Control Switch.
  5. Tap Control > Shutter Open (C) and tap Save.
  6. Tap Percentage (D) to update the percentage of shutter opening and tap Save.

  7. Tap Next.
  8. In the Automation Settings page, tap Save.

    Automation is now available under Automation tab. Use toggle switch to enable/disable automation.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?