DUG_ZB CFMT 2A_WSE-01

Using the boost mode

Using the boost mode, the setpoint is increased by 2 ºC from the current room temperature setpoint.
To use the boost mode:
  1. On the Home page, tap All devices > Thermostat.
  2. On the device control panel page, tap .
  3. In the slide-up menu, select the Boost Duration (A) and than tap Save.
    NOTE:
    • The boost duration is set to 1 hour by default.

    • Changing setpoint using during boost mode will cancel boost mode on the app

    • The boost mode will stop automatically when the boost duration is completed.

    • If the current temperature is 28.5 ºC - 29.5 ºC, then the boost mode will set the temperature to the maximum (30 ºC) temperature.

  4. To turn off the boost mode manually, go back to the control panel page and tap .
  5. In the slide-up menu, tap Off (B) and then tap Save.

    NOTE: By the end of the time counting down, the boost will be stopped automatically. If the boost feature has been turned on, and in this period there are one or more Schedule or Moment/Automation actions, the system will stop the current Boost action immediately, and perform the new actions (the new action always has a higher priority than the current action).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?