DUG_ Micro Module Light Switch_WSE-02

Pairing the device with Wiser Gateway

Using the Wiser app, first pair your device with the Wiser Gateway to access and control the device. You can either add the device manually or do an auto-scan to pair it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?