DUG_Motion Sensor_WSE-02

Replacing the batteries

To replace the batteries:
  1. Rotate the sensor counterclockwise to unlock it from the base plate.
  2. Remove the screws from the battery cover to access the batteries.
  3. Replace the batteries with proper polarity and then re-install the battery cover.
    The LED blinks green seven times and then stops blinking.
    NOTE: Make sure that the triangle mark on the battery cover and sensor are aligned.
  4. Tighten the screw that holds the sensor and its battery cover.
  5. Position the sensor on the base plate and then rotate it clockwise until it locks onto the base plate.
    IMPORTANT: Dispose used batteries, as per statutory regulations.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?