DUG_AC_Smoke alarm_WSE-00

Pairing device manually

  1. Locate the power switch on the rear side of the device. Use a screwdriver to turn the power switch to ON position.

    NOTE: When the device is mounted on a wall or on the ceiling, the power switch is automatically turned ON.
  2. In Wiser app Home page, tap +.
  3. Tap and select the required Wiser Hub on the slide-up menu.
  4. Select any one of the options to add device (A):
    • Add Device with Install Code
    • Add Device without Install Code

    TIP: It is highly recommended to pair the device with Install code.
  5. To pair the device with an install code,, tap Add Device with Install Code to display the slide-up menu. Select any one of the options (B):
    • Scan Install Code: you can scan the device for the an install code.
    • Enter Install Code Manually: you can manually enter the install code from the device.
    TIP: Install code is located on the rear side of the device.
    After scanning or entering the install code, proceed to Step 7.

  6. To pair the device without install code, tap Add Device without Install Code.
  7. Short press the Setup/Reset button 3 times.

    The LED blinks yellow.
  8. In the app, select LED is blinking yellow and tap Start Configuration (C).
  9. After a few seconds, a solid green LED indicates that the device has been successfully paired.

  10. Once the device is paired in the app, tap Done.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?