DUG_Smoke alarm DC_WSE-02

Using the device

The Control Panel of the smoke alarm allows you to view the current state of the device and allow you access the history and settings.

On the Home page, tap All devices > Smoke Alarm to access the control panel.

On the Smoke Alarm control panel page, you can see the following:


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?