DUG_Smoke alarm DC_WSE-02

Pairing the device

Using the Wiser app, pair your device with the Wiser Gateway to access and control the device. You can either add the device manually or do an auto-scan to pair it.
IMPORTANT: Do not mount the device before the pairing. The Setup/Reset button (Zigbee) and power switch are located on the rear side of the device.
NOTE: When multiple smoke alarms are paired with same Wiser Gateway, an 868MHz radio frequency (RF) interconnection is automatically created between smoke alarms.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?