SUG_Wiser_Egypt_WSE-02

Moment

One or more device actions that can be triggered together with a single command. For example, turn all the lights on and close the in the living room by tapping a button or using a voice controller such as .
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.