SUG_Wiser_Egypt_WSE-02

Blind controllers

Connected Blind Control Switch

Remotely open/close blinds or automatically set blind position in response to a specified condition or event.

Instruction Sheet (PDF)

Device User Guide

Wiser Micro Module Shades Control

Converts compatible mechanical push-button switches into smart shades switches. Connect up to 10 mechanical double push buttons.

NOTE: Mechanical push buttons must be certified for use in 220–240 V AC applications.

Instruction Sheet (PDF)

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.