DUG_Wiser_Airzone_WH-05

Using the device

In the Wiser Home app, the device control screen allows to switch ON/OFF the device and control it.

On the Control tab, select the device of which you want to access the device control screen.


The device control screen displays the following options:

A

Tap the toggle switch to allow the system to follow a schedule.

B

Tap to go to the Schedule screen, where you can edit a schedule.

C

Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide.

D

Tap to control various settings from the Device Settings screen.

E

Tap to manually turn the device ON/OFF.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.