DUG_Exxact Connected Motion Sensor with Multiwire Dimmer_WH-00

Resetting the device

You can reset the device to factory default manually.

Short press push button three times (< 0,5 s) and then long press the push button once (>10 s).
After 10 s, the LED starts blinking red, and then release the push button.

Upon successful reset, the LED stops blinking. Then, the device restarts and blinks green for a few seconds.

NOTE: After reset, the LED turns amber indicating that it is ready for pairing.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?