DUG_Exxact Single Socket Outlet_WH-01

Creating a moment

Moment allows you to group multiple actions that are usually performed together. By using the Wiser Home app, you can create moments based on your needs.
  1. On the Home screen, tap .
  2. Go to Moments > to create a moment.
  3. Enter the name of the moment (A).
    TIP: You can choose the cover image that best represents your moment by tapping .
  4. Tap Add actions (B) to select the list of devices.
  5. In the Add actions menu, you can select the devices (C).
  6. Once all the device are selected, tap Done.
  7. On the Moment creator page, tap on the device to set the condition. For example, select connected socket.
    • Tap (D) to turn on.

    When the desired condition is set, tap Set.

  8. Once all conditions are set, tap Save.
    TIP:
    • If you want to see the moments on the Home screen, go to Home > > Home Screen > Moments and enable the Moments toggle switch.

    • You can also rearrange the moments by tapping Edit from the Moments tab on the Home screen, or by tapping Automation > Moments > Reorder.

    Once the moment is saved, it is visible on the Moments tab. You can tap on the moment to enable it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?