DUG_Exxact Single Socket Outlet_WH-01

Identifying the device

Using the Wiser Home app, you can identify a Socket outlet from the other available devices in the room.
  1. On the Home screen, tap .
  2. Tap Devices > Connected Socket > Identify (A).
    NOTE:
    • This feature flashes the Socket outlet LED, so you can identify the actual device. It may take up to a minute to start and flash the Socket outlet LED.

    • The socket LED will continue to flash until you tap OK.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?