DUG_Exxact_Wireless Switch_WH-03

Controlling the device with Push Buttons

After assigning the action to the Wireless switch, you can operate it by pressing the push buttons.

Light

Short press the assigned push button on the Wireless switch (< 0,5 s) to turn the light On/Off, or set it to a specific brightness level ( for dimmers only).

Shutter

Short press the assigned push button on the Wireless switch (< 0,5 s) to open/ close the shutter to the configured percentage.

Moment

Short press the assigned push button to activate a Moment.

TIP: You can configure the Wireless switch push button with Action/Moment using the app.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?